ori


Logical sum (immediate).

[Syntax]

-

ori imm, reg1, reg2

 

The following can be specified for imm:

-

Absolute expression having a value of up to 32 bits

-

Relative expression

-

Either of the above expressions with HIGHW, LOWW, or HIGHW1 applied

[Function]

ORs the value of the absolute expression, relative expression, or expression with HIGHW, LOWW, or HIGHW1 applied specified by the first operand with the value of the register specified by the second operand, and stores the result in the register specified by the third operand.

[Description]

-

If the following is specified for imm, the assembler generates one ori machine instructionNote 1.

(a)

Absolute expression having a value in the range of 0 to 65,535

ori     imm16, reg1, reg2
ori     imm16, reg1, reg2

(b)

Relative expression having !label or %labelNote 2

ori     !label, reg1, reg2
ori     !label, reg1, reg2
ori     %label, reg1, reg2
ori     %label, reg1, reg2

(c)

Expression with HIGHW, LOWW, or HIGHW1

ori     imm16, reg1, reg2
ori     imm16, reg1, reg2

Note 1.

The ori machine instruction takes an immediate value of 0 to 65,535 (0 to 0xFFFF) as the first operand.

Note 2.

!label and %label are treated as 16-bit value (zero-extended).

 

-

If the following is specified for imm, the assembler executes instruction expansion to generate multiple machine instructions.

(a)

Absolute expression having a value in the range of -16 to -1

If reg2 is r0

ori     imm5, reg1, r0
mov     imm5, r1
or      reg1, r1

Else if reg2 is the same as reg1

ori     imm5, reg1, reg2
mov     imm5, r1
or      r1, reg2

Else

ori     imm5, reg1, reg2
mov     imm5, reg2
or      reg1, reg2

(b)

Absolute expression having a value in the range of -32,768 to -17

If reg2 is r0

ori     imm16, reg1, r0
movea   imm16, r0, r1
or      reg1, r1

Else if reg2 is the same as reg1

ori     imm16, reg1, reg2
movea   imm16, r0, r1
or      r1, reg2

Else

ori     imm16, reg1, reg2
movea   imm16, r0, reg2
or      reg1, reg2

(c)

Absolute expression exceeding the above ranges

<1>

If all the lower 16 bits of the value of imm are 0

If reg2 is r0

ori     imm, reg1, r0
movhi   HIGHW(imm), r0, r1
or      reg1, r1

Else if reg2 is the same as reg1

ori     imm, reg1, reg2
movhi   HIGHW(imm), r0, r1
or      r1, reg2

Else

ori     imm, reg1, reg2
movhi   HIGHW(imm), r0, reg2
or      reg1, reg2

<2>

Else

If reg2 is r0

ori     imm, reg1, r0
mov     imm, r1
or      reg1, r1

Else if reg2 is the same as reg1

ori     imm, reg1, reg2
mov     imm, r1
or      r1, reg2

Else

ori     imm, reg1, reg2
mov     imm, reg2
or      reg1, reg2

(d)

Relative expression having $label for a label having a definition in the sdata/sbss-attribute section

If reg2 is r0

ori     $label, reg1, r0
movea   $label, r0, r1
or      reg1, r1

Else if reg2 is the same as reg1

ori     $label, reg1, reg2
movea   $label, r0, r1
or      r1, reg2

Else

ori     $label, reg1, reg2
movea   $label, r0, reg2
or      reg1, reg2

(e)

Relative expression having #label or label, or that having $label for a label having no definition in the sdata/sbss-attribute section

If reg2 is r0

ori     #label, reg1, r0
mov     #label, r1
or      reg1, r1
ori     label, reg1, r0
mov     label, r1
or      reg1, r1
ori     $label, reg1, r0
mov     $label, r1
or      reg1, r1

Else if reg2 is the same as reg1

ori     #label, reg1, reg2
mov     #label, r1
or      r1, reg2
ori     label, reg1, reg2
mov     label, r1
or      r1, reg2
ori     $label, reg1, reg2
mov     $label, r1
or      r1, reg2

Else

ori     #label, reg1, reg2
mov     #label, reg2
or      reg1, reg2
ori     label, reg1, reg2
mov     label, reg2
or      reg1, reg2
ori     $label, reg1, reg2
mov     $label, reg2
or      reg1, reg2

[Flag]

CY

---

OV

0

S

1 if the word data MSB of the result is 1, 0 if not

Z

1 if the result is 0, 0 if not

SAT

---