< Optimizing Linkage Editor (rlink) Options / Output Options >
Specifies the maximum byte count for a data record when a file is to be created in the Intel-Hex format. Specify a one-byte hexadecimal value (01 to FF) for the byte count. When this option is not specified, the linkage editor assumes FF as the maximum byte count when creating an Intel-Hex file. |