< Optimizing Linkage Editor (rlink) Options / Output Options >
Assigns the specified address to the vector number to which no address has been assigned in the variable vector table section. |
When this option is specified, a variable vector table section is created by the linkage editor and the specified address is set in the table even if there is no interrupt function in the source code. |
This option is ignored when the user creates a variable vector table section in the source program because the variable vector table is not automatically created in this case. |