This instruction restores data from the stack and transfers it to the control register specified as dest.
-
The stack pointer in use is specified by the U bit in the PSW.
-
In user mode, writing to the ISP, INTB, BPC, BPSW, and FINTV, and the IPL[3:0], PM, U, and I bits in the PSW is ignored. In supervisor mode, writing to the PM bit in the PSW is ignored.