2.22.14 Access to the MPU area [For microcontrollers with memory-protection unit (MPU)]

The MPU area can be referred to and written to only while program execution is stopped.

If an attempt is made to access the MPU area during program execution,

-

the read data will be shown as 0x00, or

-

an error will occur if write access is attempted.

 

The following operations cannot be done in the MPU area.

-

Line assembly

-

Memory search

-

Memory cop