2.22.16 Memory access in on-chip ROM disabled extended mode

Do not read from or write to the FCU firmware area or flash-related I/O registers via the Memory or IOR panel in the on-chip ROM disabled extended mode. Otherwise bus errors will occur.