2.22.17 Event combination condition [RX71M, RX64M, RX651, RX65N]

When the event combination condition is set to [Sequential], do not specify events for consecutive instructions.

Events may not occur depending on the instruction type.