2.22.2 FINE interface

-

The external trace output and real-time RAM monitor functions via FINE interface are not supported.

-

Hot plug-ins via FINE interface are not supported.

 

[RX62x, RX630, RX631, RX63N, RX63T, RX634]

-

The FINE interface supports only a two-wire system making use of FINEC and MD/FINED pins. One-wire systems are not supported.

 

[RX71M, RX651, RX65N, RX64M, RX210, RX21A, RX220, RX23x, RX24T, RX110, RX111, RX113, RX130]

-

The FINE interface supports a one-wire system making use of MD/FINED pin.