Halts the clock supplied to the serial interface IICA.
Remark | Calling this API function changes the serial interface IICA to reset status.
For this reason, writes to the control registers (e.g. IICA control register n: IICCTLn) after this API function is called are ignored.
|
[Syntax]
void R_IICAn_Set_PowerOff ( void );
|
Remark | n is the channel number. |
[Argument(s)]
None.
[Return value]
None.