|
|
R_IICAn_Create
|
Performs initialization necessary to control the serial interface IICA.
|
R_IICAn_Create_UserInit
|
Performs user-defined initialization related to the serial interface IICA.
|
r_iican_interrupt
|
Performs processing in response to the IICA communication end interrupt INTIICAn.
|
R_IICAn_StopCondition
|
Generates stop conditions.
|
R_IICAn_Stop
|
Ends IICA communication.
|
R_IICAn_Reset
|
Reset the serial interface IICA.
|
R_IICAn_Set_PowerOff
|
Halts the clock supplied to the serial interface IICA.
|
R_IICAn_Master_Send
|
Starts IICA master transmission.
|
R_IICAn_Master_Receive
|
Starts IICA master reception.
|
r_iican_callback_master_sendend
|
Performs processing in response to the IICA master transmission end interrupt INTIICAn.
|
r_iican_callback_master_receiveend
|
Performs processing in response to the IICA master reception end interrupt INTIICAn.
|
r_iican_callback_master_error
|
Performs processing in response to detection of IICA master communication error.
|
R_IICAn_Slave_Send
|
Starts IICA slave transmission.
|
R_IICAn_Slave_Receive
|
Starts IICA slave reception.
|
r_iican_callback_slave_sendend
|
Performs processing in response to the IICA slave transmission end interrupt INTIICAn.
|
r_iican_callback_slave_receiveend
|
Performs processing in response to the IICA slave reception end interrupt INTIICAn.
|
r_iican_callback_slave_error
|
Performs processing in response to detection of IICA slave communication error.
|
r_iican_callback_getstopcondition
|
Performs processing in response to detection of stop condition.
|
R_IICAn_Set_SnoozeOn
|
Enables operation of the address match wakeup function in STOP mode.
|
R_IICAn_Set_SnoozeOff
|
Disables operation of the address match wakeup function in STOP mode.
|
R_IICAn_Set_WakeupOn
|
Enables operation of the address match wakeup function in STOP mode.
|
R_IICAn_Set_WakeupOff
|
Disables operation of the address match wakeup function in STOP mode.
|