r_iican_callback_master_error


Performs processing in response to detection of IICA master communication error.

[Syntax]

#include    "r_cg_macrodriver.h"
static  void    r_iican_callback_master_error ( MD_STATUS flag  );

Remark

n is the channel number.

[Argument(s)]

I/O

Argument

Description

I

MD_STATUS flag;

Cause of communication error

MD_SPT: Stop condition detected

MD_NACK: Acknowledge not detected
(No slave that matches the address/A slave can receive no more data or does not require the next data)

[Return value]

None.