r_iican_callback_slave_sendend


Performs processing in response to the IICA slave transmission end interrupt INTIICAn.

Remark

This API function is called as the callback routine of interrupt process r_iican_interrupt corresponding to the IICA slave transmission end interrupt INTIICAn.

[Syntax]

static  void    r_iican_callback_slave_sendend ( void );

Remark

n is the channel number.

[Argument(s)]

None.

[Return value]

None.