R_RTC_Set_BinaryCounterValue


Sets the counter value of the real-time clock.(in the case of the binary mode setting)

[Syntax]

#include    "r_cg_macrodriver.h"
#include    "r_cg_rtc.h"
MD_STATUS   R_RTC_Set_BinaryCounterValue ( uint32_t counter_write_val );

[Argument(s)]

I/O

Argument

Description

I

uint32_t
  counter_write_val;

Counter value

Remark

See R_RTC_Set_CounterValue for details about the rtc_counter_value_t counter value.

[Return value]

Macro

Description

MD_OK

Normal completion

MD_BUSY1

Executing count process (before change to setting)

Remark

If MD_BUSY1 is returned, it may be because the counter operation start wait time is too short, so make the value of the RTC_WAITTIME macro defined in the header file "r_cg_rtc.h" larger.