Reads the counter value of the real-time clock.(in the case of the binary mode setting)
#include "r_cg_macrodriver.h" #include "r_cg_rtc.h" MD_STATUS R_RTC_Get_BinaryCounterValue ( uint32_t * const counter_read_val ); |
uint32_t * const counter_read_val; |
Pointer to structure in which to store the counter value being read |