|
|
|
|
R_RTC_Create
|
Performs initialization necessary to control the real-time clock.
|
|
R_RTC_Create_UserInit
|
Performs user-defined initialization relating to the real-time clock.
|
|
r_rtc_interrupt
|
Performs processing in response to the real-time clock interrupt INTRTC.
|
|
R_RTC_Start
|
Starts the count of the real-time clock (year, month, weekday, day, hour, minute, second).
|
|
R_RTC_Stop
|
Ends the count of the real-time clock (year, month, weekday, day, hour, minute, second).
|
|
R_RTC_Set_PowerOff
|
Halts the clock supplied to the real-time clock.
|
|
R_RTC_Set_HourSystem
|
Sets the clock type (12-hour or 24-hour clock) of the real-time clock.
|
|
R_RTC_Set_CounterValue
|
Sets the counter value of the real-time clock.
|
|
R_RTC_Set_CalendarCounterValue
|
Sets the counter value of the real-time clock.(in the case of the calendar mode setting)
|
|
R_RTC_Set_BinaryCounterValue
|
Sets the counter value of the real-time clock.(in the case of the binary mode setting)
|
|
R_RTC_Get_CounterValue
|
Reads the counter value of the real-time clock.
|
|
R_RTC_Get_CalendarCounterValue
|
Reads the counter value of the real-time clock.(in the case of the calendar mode setting)
|
|
R_RTC_Get_BinaryCounterValue
|
Reads the counter value of the real-time clock.(in the case of the binary mode setting)
|
|
R_RTC_Set_ConstPeriodInterruptOn
|
Sets the cycle of the interrupts INTRTC, then starts the cyclic interrupt function.
|
|
R_RTC_Set_ConstPeriodInterruptOff
|
Ends the cyclic interrupt function.
|
|
r_rtc_callback_constperiod
|
Performs processing in response to the cyclic interrupt INTRTC.
|
|
R_RTC_Set_AlarmOn
|
Starts the alarm interrupt function.
|
|
R_RTC_Set_CalendarAlarmOn
|
Starts the alarm interrupt function.(in the case of the calendar mode setting)
|
|
R_RTC_Set_BinaryAlarmOn
|
Starts the alarm interrupt function.(in the case of the binary mode setting)
|
|
R_RTC_Set_AlarmOff
|
Ends the alarm interrupt function.
|
|
R_RTC_Set_AlarmValue
|
Sets the alarm conditions (weekday, hour, minute).
|
|
R_RTC_Set_CalendarAlarmValue
|
Sets the alarm conditions (year, month, weekday, day, hour, minute, second).(in the case of the calendar mode setting)
|
|
R_RTC_Set_BinaryAlarmValue
|
Sets the alarm conditions.(in the case of the binary mode setting)
|
|
R_RTC_Get_AlarmValue
|
Reads the alarm conditions (weekday, hour, minute).
|
|
R_RTC_Get_CalendarAlarmValue
|
Reads the alarm conditions (year, month, weekday, day, hour, minute, second).(in the case of the calendar mode setting)
|
|
R_RTC_Get_BinaryAlarmValue
|
Reads the alarm conditions.(in the case of the binary mode setting)
|
|
r_rtc_callback_alarm
|
Performs processing in response to the alarm interrupt INTRTC.
|
|
R_RTC_Set_RTC1HZOn
|
Enables output of the correction clock (1 Hz) to the RTC1HZ pin.
|
|
R_RTC_Set_RTC1HZOff
|
Disables output of the correction clock (1 Hz) to the RTC1HZ pin.
|
|
R_RTC_Set_RTCOUTOn
|
Enables output of the RTCOUT.
|
|
R_RTC_Set_RTCOUTOff
|
Disables output of the RTCOUT.
|
|
r_rtc_alarminterrupt
|
Performs processing in response to the alarm interrupt INTRTCALM.
|
|
r_rtc_periodicinterrupt
|
Performs processing in response to the periodic interrupt INTRTCPRD.
|
|
r_rtc_callback_periodic
|
Performs processing in response to the cyclic interrupt INTRTC.
|