|
R_RTC_Set_BinaryAlarmValue
|
Sets the alarm conditions.(in the case of the binary mode setting)
[Syntax]
#include "r_cg_macrodriver.h"
#include "r_cg_rtc.h"
void R_RTC_Set_BinaryAlarmValue ( uint32_t alarm_enable, uint32_t alarm_val );
|
[Argument(s)]
|
|
|
|
|
|
uint32_t alarm_enable;
|
Alarm enable
(Set the value to the Binary Counter Alarm Enable Register)
|
|
|
uint32_t alarm_val
|
Alarm conditions (count value)
(Set the value to the Binary Counter Alarm Register)
|
[Return value]
None.