Renesas Electronics
Configure the operating environment on the Property panel below when using E1.
Figure 2.23
Example of Property Panel [E1]
Follow the steps below by selecting the corresponding tab on the Property panel.
2.3.3.1 [Connect Settings] tab
2.3.3.2 [Debug Tool Settings] tab
2.3.3.3 [Download File Settings] tab
2.3.3.4 [Hook Transaction Settings] tab