2.3.4 [E20]

Configure the operating environment on the Property panel below when using E20.

Figure 2.31

Example of Property Panel [E20]

 

Follow the steps below by selecting the corresponding tab on the Property panel.

 

2.3.4.1 [Connect Settings] tab

2.3.4.2 [Debug Tool Settings] tab

2.3.4.3 [Download File Settings] tab

2.3.4.4 [Hook Transaction Settings] tab