Renesas Electronics
Configure the operating environment on the Property panel below when using EZ Emulator.
Figure 2.38
Example of Property Panel [EZ Emulator]
Follow the steps below by selecting the corresponding tab on the Property panel.
2.3.5.1 [Connect Settings] tab
2.3.5.2 [Debug Tool Settings] tab
2.3.5.3 [Download File Settings] tab
2.3.5.4 [Hook Transaction Settings] tab