2.4.4  
Remove a subproject from the project
 
To remove a subproject registered to a project from that project, select the Subproject node on the project tree, and select [Remove from Project] on the context menu.
In addition, the subproject file itself is not deleted from the file system.
| 
Figure 2.21 | [Remove from Project] Item |