2.4.6 Open a project folder in Explorer

You can open the folder where the project file for a project (main project or subproject) is saved from the project tree in Explorer.

Select the Project node or Subproject node and select [Open Folder with Explorer] on the context menu.

Figure 2.23

[Open Folder with Explorer] Item (For a Project)

 

Remark

When you select [Open Folder with Explorer] from a file's context menu, the folder the file is saved in is opened in Explorer.