2.4.8 Open a CubeSuite+ project

A CubeSuite+ project whose build tool is lower than CC-RX V2.02.00 or lower than CC-RH V1.01.00 can also be opened from CS+ with the following method.

(1)

Install the compiler package

Copy the compiler folder of the relevant version from the CubeSuite+ installation folder and paste it to the CS+ installation folder.

 

Copy from: CubeSuite+ install folder\CubeSuite+\CC-XX\Vx.xx

Paste to: CS+ install folder\CC\CC-XX

Caution

This operation must be conducted with administrator privileges of Windows.

(2)

Open the CubeSuite+ project

Select [Open Project...] from the [Project] menu with CS+, and then select a CubeSuite+ project file (see "(1) Open an existing project").

(3)

Set the version of the compiler package

Select the target version in the [Using compiler package version] property of the build tool (see "2.5 Change the Build Tool Version").

Caution

When the compiler package is installed with the above method, it cannot be uninstalled by the integrated uninstaller. Delete all copied folders from Explorer, etc. to uninstall the compiler package.