Column Chooser dialog box


This dialog box is used to sort, show/hide the items (columns) displayed on the Function List panel/Variable List panel.

If the Customize Display Method operation has been performed on one of the panels, then this dialog can also be used to reset these customizations to the default settings.

Figure A.43

Column Chooser Dialog Box (For Function List Panel)

Figure A.44

Column Chooser Dialog Box (For Variable List Panel)

 

The following items are explained here.

[How to open]

-

On the Function List panel, click the button.

-

On the Variable List panel, click the button.

[Description of each area]

(1)

Item list area

This area displays a list of all items (columns) that can be displayed in the Function List panel/Variable List panel (the items (columns) that can be displayed differ according to the microcontroller and the debug tool used).

The display order of the items in this list, and the state of checkboxes, are the same as the current sort order and visible/hidden status in the corresponding panel.

Specify the check boxes of each item to show or hide that item on the panel.

 

Displays this item on the panel.

 

Does not display this item on the panel.

 

Indicates that a message relating to information about this item has been output to the Output panel. Hover the mouse over it to display a pop-up with the last message to be output.

[Function buttons]

Button

Function

Default

Resets the display order and visible/hidden settings for each item in the Function List panel/Variable List panel to their default valuesNote.

Note that all display locking, display filtering, and other customization will be cleared.

Close

Closes this dialog box.

Note

The default display status for each item is as follows:
The order of [Item] in the table corresponds to the display order of items (columns) on each panel.
Note that items displayed differ depending on the microcontroller and debug tool used (see "(2) Information area" of the Function List panel/"(2) Information area" of the Variable List panel).

Table A.5

Default Display Status (Function List Panel)

Item

Status

While Disconnecting from Debug Tool

While Connecting to
Debug Tool

Function Name

Display

Display

Class Name

Display

Display

Namespace

Non-display

Non-display

File Name

Display

Display

File Path

Non-display

Non-display

PM Information [RH850]

Display

Display

Import

Non-display

Non-display

Access Specifier

Display

Display

Attribute

Display

Display

Return Type

Display

Display

Arguments Count

Non-display

Non-display

Arguments

Display

Display

Code Size[Bytes]

Display

Display

Start Address

Display

Display

End Address

Non-display

Non-display

Reference Count

Display

Display

Execution Count

Non-display

Display

Execution Time[unit]

Non-display

Display

Execution Time(Percentage)[%]

Non-display

Display

Execution Time(Average)[unit]

Non-display

Display

Code Coverage[%]

Non-display

Display

Table A.6

Default Display Status (Variable List Panel)

Item

Status

While Disconnecting from Debug Tool

While Connecting to
Debug Tool

Variable Name

Display

Display

Class Name

Display

Display

Namespace

Non-display

Non-display

File Name

Display

Display

Function Name

Non-display

Non-display

File Path

Non-display

Non-display

PM Information [RH850]

Non-display

Display

Import

Non-display

Non-display

Access Specifier

Display

Display

Attribute

Display

Display

Type

Display

Display

Members

Display

Display

Address

Display

Display

Size[Bytes]

Display

Display

Reference Count

Display

Display

Read Count

Non-display

Display

Write Count

Non-display

Display

Read/Write Count

Non-display

Non-display

Minimum Value

Non-display

Display

Maximum Value

Non-display

Display

Data Coverage[%]

Non-display

Display