Project Tree panel


This panel is used to display components of the project (microcontroller, design tool, build tool, debug tool, etc.) in a tree structure.

Figure A.2

Project Tree Panel

 

The following items are explained here.

[How to open]

-

From the [View] menu, select [Project Tree].

[Description of each area]

(1)

Project tree area

Project components are displayed in tree view with the following given node.

Node

Description

Program Analyzer (Analyze Tool)

This is the analysis tool to use.

Remark

When the node is selected, the detailed information (property) is displayed in the Property panel, and you can change the settings.
The Property panel can be opened by double-clicking on the node when the Property panel is not opened.

[Context menu]

The following context menu items are displayed by right clicking the mouse on [Program Analyzer (Analyze Tool)] node.

Function List

Opens the Function List panel.

Variable List

Opens the Variable List panel.

Analysis Chart

Opens the Analysis Chart panel.

Call Graph

Opens the Call Graph panel.

Class/Member

Opens the Class/Member panel.

Property

Opens the Property panel containing the information for the analysis tool.