A.1 Description

The analysis tool has the following windows, panels and dialog boxes.

Table A.1

Window/Panel/Dialog Box List

Window/Panel/Dialog Box Name

Description

Main window

This is the first window to open when CS+ is launched.

Project Tree panel

Displays the components of the project in a tree structure.

Property panel

Displays detailed information on the analysis tool and changes the settings of the information.

Function List panel

Displays the acquired function information.

Variable List panel

Displays the acquired variable information.

Analysis Chart panel

Displays charts of the acquired function information and variable information.

Call Graph panel

Displays calling relationships between functions (call graph).

Class/Member panel

Displays the acquired class information [CC-RX]Note, function information and variable information in a tree structure.

Variable Value Changing Chart (zoomed in) panel

Zooms in on the specified range on the chart.

Output panel

Displays operation logs for various components provided by CS+ and the reference list for functions/variables.

Select Files not To Analyze dialog box

Specifies files not to analyze.

Select Files To Analyze dialog box

Specifies files to analyze.

Column Chooser dialog box

Changes the order of the display items and the setting of display/non-display for the Function List panel/Variable List panel.

Call Graph Search dialog box

Searches for a function/variable exists in the call graph displayed in the Call Graph panel.

Filter Settings dialog box

Specifies the filter conditions to display the information on the Function List panel/Variable List panel.

Note

[CC-RX]

The class information is provided only when C++ source files are subject to analysis.