R_RIICn_StopCondition


Issues the stop condition and causes a transfer error and an event generation interrupt (EEI).

Remark

r_riicn_error_interrupt is called in response to calling of this API function.

[Syntax]

void    R_RIICn_StopCondition ( void );

Remark

n is the channel number.

[Argument(s)]

None.

[Return value]

None.