Performs processing in response to the transfer error/event generation interrupts (EEI).
This API function is called to run interrupt processing for the transfer error/event generation interrupts (EEI), which are generated when the I2C bus interface detects the transfer error/event generation (arbitration-lost, NACK, timeout, start condition, and stop condition). |