r_riicn_receive_interrupt
|
Performs processing in response to the receive data full interrupts (RXI).
Remark | This API function is called to run interrupt processing for the receive data full interrupts (RXI). |
[Syntax]
static void r_riicn_receive_interrupt ( void );
|
Remark | n is the channel number. |
[Argument(s)]
None.
[Return value]
None.