Of the internal processing for transfer errors and event generation interrupts (EEI), this function handles processing specialized in the arbitration-lost detection, NACK detection, and timeout detection.
This API function is called as the r_riicn_error_interrupt callback routine. |
MD_STATUS status; |
Source of the transfer errors and event generation interrupts |