ceilf.dw


Conversion to fixed-point format (double precision) (Floating-point Convert Double to Word, round toward positive (Double))

[Syntax]

-

ceilf.dw reg1, reg2

[Function]

This instruction arithmetically converts the double-precision floating-point format contents of the register pair specified by general-purpose register reg1 to 32-bit fixed-point format, and stores the result in general-purpose register reg2.

The result is rounded in the +∞ direction regardless of the current rounding mode.

When the source operand is infinite or not-a-number, or when the rounded result is outside the range of 231 - 1 to -231, an IEEE754-defined invalid operation exception is detected.

If invalid operation exceptions are not enabled, the preservation bit (bit 4) of the FPSR register is set as an invalid operation and no exception occurs. The return value differs as follows, according to differences among sources.

-

Source is a positive number or +∞ : 231 - 1 is returned.

-

Source is a negative number, not-a-number, or -∞ : -231 is returned.

[Description]

-

The assembler generates one ceilf.dw machine instruction.