Rearrange Commands dialog box


This dialog box allows you to change the arrangement (including addition and deletion) of menu items and buttons in the Main window.

Figure A.67

Rearrange Commands Dialog Box

 

The following items are explained here.

[How to open]

-

In the [Commands] tab of the User Setting dialog box, click the [Rearrange Commands...] button.

[Description of each area]

(1)

[Choose a menu or toolbar to rearrange] area

This area allows you to specify the item whose position you want to change.

First select the [Menu Bar] if you want to change the menu item or [Toolbar] if you want to change the toolbar button using the option button, and then select the category to be changed from the drop-down list.

(2)

[Commands] area

This area displays a list of commands belonging to the category selected in the [Choose a menu or toolbar to rearrange] area which will be displayed in the Main window.

You can change the arrangement of these commands using the following buttons in this area.

Add...

Opens the Add Command Dialog Box for selecting a command to be added above the command currently selected in this area.

In the Add Command Dialog Box, all commands that can be added are displayed, grouped by their categories.

First select the category of command in the [Categories] area, then select the command you want to add and press the [OK] button (pressing the [Cancel] button cancels the addition of the command and closes this dialog box).

Delete

Deletes the command currently selected in this area.

Move Up

Moves the command currently selected in this area up one line.

Move Down

Moves the command currently selected in this area down one line.

Modify Selection

Displays the following menu items for editing the arrangement of the menu item or button currently selected in this area.

Menu Item

Description

Reset

Resets the selected menu item/button.

Delete

Deletes the selected menu item/button.

Name

Displays the name of the selected menu item/button.

Default Style

Checking this menu item returns the display style of the selected menu item/button to the default state (by default).

Text Only (Always)

Checking this menu item displays the selected menu item/button by text only (the icon will not be displayed).

Text Only (in Menus)

This is enabled only when a menu item is selected. Checking this menu item displays the selected menu item/button by text only (the icon will not be displayed).

Image and Text

Checking this menu item displays the selected menu item/button by both text and icon.

Begin a Group

Inserts separator just before the selected menu item/button.

Recently Used

This item is not supported in this version.

Figure A.68

Add Command Dialog Box

[Function buttons]

Button

Function

Reset...

Restores the arrangement of menu items or toolbar buttons belonging to the category currently selected in the [Choose a menu or toolbar to rearrange] area to its default state.

Close

Finishes the arrangement of commands and closes this dialog box.