This dialog box is used to display messages output by the various tools.
The following items are explained here.
Shows messages to inform in icons and message information (edit not allowed).
Note that the message is categorized by the following message types and an alphabet to indicate the message type is added to the head of the ID number.
[Direct message type Cause] only appears when there are details for the message output.
Refer to the message displayed in [Direct message type Cause] and its help if you are unable to identify the cause of the issue from the message output and its help.
The message types may differ; for example, the type of the message output may be a warning, while the direct cause is a fatal error. |
This area displays the information only when there is detailed information in the output message. To display this area, click [Detail] button (the area is not displayed as default).
The details of the output message are displayed in tree view categorized by items (edit not allowed).
When displaying it, the following icon is added.
[[Edit] menu (Message dialog box-dedicated items)]
The following items are exclusive to [Edit] menu in Message dialog box (other items are all invalid).
The following items are exclusive to [Edit] menu in Message dialog box (other items are all invalid).
Display/hide the detailed display area. Note that this button is available only when there is detailed information. |
|||
Saves a snapshot of the window and error information on the desktop. These files would help us to reply more quickly and efficiently when you contact us. |
|||
Displays the help with regard to the displayed message. And a Web browser is displayed and a search for FAQs with regard to the message is started.
Use the offline help. (From the [Help] menu, select [How to Access Help] >> [Offline].) Hide FAQs. (Clear the [Search FAQ when the help of a message opens.] check box in the [General - Smart Browser] category of the Option dialog box.) FAQs can be searched on the Smart Browser panel. Enter the message number, etc. in the text box and click the [Search FAQ] button. |