r_kb2m_interrupt

Performs processing in response to the timer interrupt INTTKB2m.

Remark This API function is called as the interrupt process corresponding to the timer interrupt INTTKB2m.

[Syntax]

CA78K0R Compiler

__interrupt static void r_kb2m_interrupt ( void );

CC-RL Compiler

static void __near r_kb2m_interrupt ( void );

Remark m is the unit number.

[Argument(s)]

None.

[Return value]

None.