R_KB2m_TKBOn1_SmoothStartFunction_Stop

Ends smooth start function for timer output TKBOn1.

[Syntax]

void R_KB2m_TKBOn1_SmoothStartFunction_Stop ( void );

Remark m is the unit number, and n is the channel number.

[Argument(s)]

None.

[Return value]

None.