R_KB2m_TKBOn0_Forced_Output_Stop_Function1_Stop

Ends forced output stop function 1 for timer output TKBOn0.

[Syntax]

void R_KB2m_TKBOn0_Forced_Output_Stop_Function1_Stop ( void );

Remark m is the unit number, and n is the channel number.

[Argument(s)]

None.

[Return value]

None.