R_KB2m_TKBOn1_Forced_Output_Stop_Function1_Start

Starts forced output stop function 2 for timer output TKBOn1.

[Syntax]

void R_KB2m_TKBOn1_Forced_Ourput_Stop_Function1_Start ( void );

Remark m is the unit number, and n is the channel number.

[Argument(s)]

None.

[Return value]

None.