-ROm


This option specifies the section that maps symbols from ROM to RAM.

[Specification format]

-ROm=ROMsection=RAMsection[,ROMsection=RAMsection]...

 

-

Interpretation when omitted

None

[Detailed description]

-

This option reserves ROM and RAM areas in the initialized data area and relocates defined symbols in the ROM section with the address in the RAM section.

-

Specify a relocatable section including the initial value for ROM section ROMsection.

-

Specify a a nonexistent section or relocatable section whose size is 0 for RAM section RAMsection.

[Example of use]

-

To reserve the .data.R section with the same size as the .data section and relocate defined symbols in the .data section with address in the .data.R section, describe as:

>rlink a.obj b.obj -rom=.data=.data.R -start=.data/100,.data.R/FAF00

[Remark]

-

If the -form={object|relocate|library} option, -strip option, or -extract option is specified, this option will be invalid.