-SPLIT_VECT [V1.07 or later]


This option generates vector table sections split by vector table address.

[Specification format]

-SPLIT_VECT

 

-

Interpretation when omitted

None

[Detailed description]

-

This option generates vector table sections split by vector table address.

-

A vector table section is not generated for an unused area of the vector table address.

[Example of use]

-

To generate a vector table section ".vect14" for vector table address 0x14, code as:

>rlink a.obj b.obj –vectn=14=__dummy -split_vect

[Remark]

-

If the -vect option is specified, this option will be invalid.

-

If the -form={object | relocate | library} option, -strip option, or -extract option is specified, this option will be invalid.