< Compile Options / Optimize Options >
This option is not available in V.2.00. Any specification of this option will simply be ignored and will not lead to an error due to compatibility with former versions. |
For C (C99) source files, -merge_files can be used instead of -file_inline. Add the file that was used with -file_inline (including the file path if -file_inline_path was used together with it) as one of the source files to be merged. |