< Compile Options / Optimize Options >
[Format]
The default for this option is nomap when the optimize=0, optimize=1, or optimize=2 option has been specified.
[Description]
- | When the nomap option is specified, accesses to external variables are not optimized. |
[Example]
long A,B,C;
void func()
{
A = 1;
B = 2;
C = 3;
}
|
_func:
MOV.L #_A,R4
MOV.L #1,[R4]
MOV.L #_B,R4
MOV.L #2,[R4]
MOV.L #_C,R4
MOV.L #3,[R4]
|