< Compile Options / Optimize Options >
[Format]
If this option is omitted, optimization of modification of the operation order in a floating-point expression is not performed.
[Description]
- | This option is not available in V.2.00. Any specification of this option will simply be ignored and will not lead to an error due to compatibility with former versions. |