< Optimizing Linkage Editor (rlink) Options / Output Options >
When this option is omitted, various data records are output according to each address.
| If there is an address that is larger than the specified data record, the appropriate data record is selected for the address. |