-byte_count


< Optimizing Linkage Editor (rlink) Options / Output Options >

[Format]

-byte_count=<numerical value>

 

-

[Default]

The default values are FF (hexadecimal) for Intel HEX-format files and 10 (hexadecimal) for Motorola S-format files.

[Description]

-

This option is used to specify the length of data records in Intel HEX-format files or Motorola S-format files to be generated.

-

Values from 01 to FF (hexadecimal) are specifiable for Intel HEX-format files.

-

The following ranges of values are specifiable for Motorola S-format files.

-

S1 records: 01 to FC (hexadecimal)

-

S2 records: 01 to FB (hexadecimal)

-

S3 records: 01 to FA (hexadecimal)

[Examples]

Specifying 16 bytes (10 in hexadecimal) as the length of data records

-byte_count=10

[Remarks]

-

This option is invalid for file formats other than Intel HEX type (form=hex) or Motorola S-record type (form=stype).