< Optimizing Linkage Editor (rlink) Options / Output Options >
[Format]
-rom = <suboption>[,...]
<suboption>: <ROM section name>=<RAM section name>
|
[Description]
- | Reserves ROM and RAM areas in the initialized data area and relocates a defined symbol in the ROM section with the specified address in the RAM section. |
- | Specifies a relocatable section including the initial value for the ROM section. |
- | Specifies a nonexistent section or relocatable section whose size is 0 for the RAM section. |
[Examples]
rom=D=R
start=D/100,R/8000
|
- | Reserves R section with the same size as D section and relocates defined symbols in D section with the R section addresses. |
[Remarks]
- | When form={object | relocate | library}or strip is specified, this option is unavailable. |