|
r_atuiv_timerknm_callback_overflow
|
Performs processing in response to the overflow interrupt.
Remark | This API function is called as the callback routine of interrupt process r_atuiv_timerknm_interrupt corresponding to the overflow interrupt. |
[Syntax]
void r_atuiv_timerknm_callback_overflow_callback ( void );
|
Remark | k is the timer kind, n is the unit number, m is the channel number. |
[Argument(s)]
None.
[Return value]
None.