|
R_ATUIV_Timerknm_Get_Measure_Value
|
Reads the value of measurement (number of edges, off-state duty cycle, PWM cycle, edge input time).
[Syntax]
void R_ATUIV_Timerknm_Get_Measure_Value ( uint16_t * edge, uint32_t * off_duty_cycle, uint32_t * pwm_cycle, uint32_t * edge_input_time );
|
Remark | k is the timer kind, n is the unit number, m is the channel number. |
[Argument(s)]
|
|
|
|
|
|
uint16_t * edge;
|
Pointer to area in which to store the number of edges
|
|
|
uint32_t * off_duty_cycle;
|
Pointer to area in which to store the off-state duty cycle
|
|
|
uint32_t * pwm_cycle;
|
Pointer to area in which to store the PWM cycle
|
|
|
uint32_t * edge_input_time;
|
Pointer to area in which to store the edge input time
|
[Return value]
None.