R_ATUIV_Timerknm_Set_Compare_Match


Sets the compare match register.

[Syntax]

void    R_ATUIV_Timerknm_Set_Compare_Match ( void );

Remark

k is the timer kind, n is the unit number, m is the channel number.

[Argument(s)]

None.

[Return value]

None.