R_ATUIV_Timerknm_Set_One_Shot_Pulse


Renewal the one shot pulse register.

[Syntax]

void    R_ATUIV_Timerknm_Set_One_Shot_Pulse ( void );

Remark

k is the timer kind, n is the unit number, m is the channel number.

[Argument(s)]

None.

[Return value]

None.