3.2.2 Clock controller

Below is a list of API functions output by the Code Generator for clock controller (include reset function, on-chip debug function, etc.) use.

Table 3.2

API Functions: [Clock controller]

API Function Name

Function

R_CGC_Create

Performs initialization required to control the clock generator (include reset function, on-chip debug function, etc.).

R_CGC_Create_UserInit

Performs user-define initialization relating to the clock generator (include reset function, on-chip debug function, etc.).

R_CGC_CK_Output_Enable

Enables output of the CK pin.

R_CGC_CK_Output_Enable

Disables output of the CK pin.