3.2.24 Key Return

Below is a list of API functions output by the Code Generator for key return use.

Table 3.24

API Functions: [Key Return]

API Function Name

Function

R_KEY_Create

Performs initialization necessary to control the key return functions.

R_KEY_Create_UserInit

Performs user-defined initialization relating to the key return functions.

r_key_interrupt

Performs processing in response to the key return interrupt.

R_KEY_Start

Enables the acceptance of the key return interrupt.

R_KEY_Stop

Disables the acceptance of the key return interrupt.